Configure the Advanced OPC Server

For every OPC server with which you want ClearSCADA to communicate using the OPC protocol, you need to configure an Advanced OPC Server in the ClearSCADA database.

Before configuring an Advanced OPC Server in the database, carry out any necessary Preparation. Then use the fields on the Advanced OPC Server Form to configure the item(s) on your system.

The Form has several tabs. This topic explains about the properties that are on the Server tab. Properties on other tabs are common to many database items, see Tabs That are Common to Many Configuration Forms in the ClearSCADAGuide to Advanced Drivers.

Use the fields on the Server tab to define the connection properties that are required for successful communications with the node on which the OPC DA server data is located.

For information about configuring the properties within the following sections of the Server tab, select the relevant link below:

For information on the minimum amount of configuration that you can undertake to produce a functional Advanced OPC Server in ClearSCADA, see Minimum Server Configuration.


Disclaimer

ClearSCADA 2017 R3