Configuring Advanced OPC Digital Points

Use an Advanced OPC Digital Point to map an item within the OPC DA server onto a digital point in the ClearSCADA database. The item should have an appropriate data type for a digital point.

Configure the properties of each digital point using the fields on the Advanced OPC Digital Point Form.

This section covers configuration of the digital-specific properties on the Digital Point tab of the Form.

Use the Digital Point tab to:

For information on the Control tab, see Define the Control Settings for a Digital Output Point and see Update an Output Point Value on Successful Action.

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the ClearSCADA Guide to Core Point Configuration).

Properties on other tabs are common to many points, see Tabs on Point Forms in the ClearSCADAGuide to Advanced Drivers.


Disclaimer

ClearSCADA 2017 R3