Enable Group

Associated with: Advanced OPC Groups

Security permission required to access this pick action: Disable Points

Use the Enable Group pick action to place an Advanced OPC Group In Service. Triggering the action changes the Group's configuration so that the In Service property is enabled. Providing that the items associated with the Group are also In Service and have valid configuration, they will become active.

The Enable Group pick action is only available for an OPCGroup:

NOTE: If using this pick action with the Automation Interface, you need to specify the method name Enable.


Disclaimer

ClearSCADA 2017 R3