Introduction to the Advanced OPC Driver

This driver is an advanced driver. It provides additional functionality to enable ClearSCADA to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is intended for use by engineers who are responsible for the configuration of OPC-specific items and features in ClearSCADA. It can also be used by system administrators when investigating unexpected behavior relating to the Advanced OPC driver and operators who access the configured items.

Document Scope

The Advanced OPC driver is an OPC Data Access (DA) client. OPC DA is a standard defined by the OPC Foundation and is based OLE/COM interfaces, which allows interoperability between automation/control applications, field systems/devices, and business/office applications in the process control industry. ClearSCADA supports the OPC DA versions 1.0, 2.0 and 3.0 standard to allow transfer of data between the ClearSCADA server and third-party OPC DA servers.

The Advanced OPC driver is used to read and write to data on other servers, including ClearSCADA or third-party servers, using the OPC protocol. The driver supports private security that may be required to access particular items in an OPC DA server.

This guide explains how to configure OPC-specific features and items within the ClearSCADA database (see Configuring Advanced OPC Items).

It also explains driver-specific aspects that are of interest to system administrators and engineers when investigating unexpected system behavior relating to the Advanced OPC driver (see OPC Server Registration and Server Browsing, and see Advanced OPC Specific Status Display Attributes.)

There are driver-specific pick actions for items on the Advanced OPC driver (Using Advanced OPC Specific Actions). In addition, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).

ClearSCADA includes three drivers: Simple OPC, Advanced OPC and OPC XML-DA — for information on which driver is appropriate for your system requirements, see Which OPC Driver?

Further Information

OPC Foundation Standards: see www.opcfoundation.org

OPC Time Formats used in ClearSCADA: see Using OPC Time Formats.


Disclaimer

ClearSCADA 2017 R3