Configure the Advanced Trio Diagnostic Properties that are Specific to Digital Points

D Series radios provide support for interrogation of fewer diagnostics parameters than other supported radio series. To retrieve an item of diagnostics data from a D Series radio, you associate that data with a Trio Diagnostics Analog Point; other types of point are not used to retrieve diagnostics data from D Series radios.

Use the fields on the Digital Point tab to configure the digital point properties that are specific to the Advanced Trio Diagnostics driver. Some of the fields are common to many Advanced Trio Diagnostics points (see Configure the Common Point Properties). Fields that are specific to Advanced Trio Diagnostics Digital Input points and Digital Output points are explained below.

Further Information

Persistence: see Use Persistence to Stop Fleeting Changes in Value from Changing a Point State.

The other properties on the Digital Point tab that are not shown in the above figure are common to digital points on many drivers. For information on the fields, see Defining Digital Point Details in the ClearSCADA Guide to Core Point Configuration.


Disclaimer

ClearSCADA 2017 R3