Configuring an Advanced Trio Diagnostics Radio Channel

You use an Advanced Trio Diagnostics Radio Channel in the database to represent a communication connection between the ClearSCADA server and a Trio radio (or hot-standby controller unit, in the case of a hot-standby radio setup).

To create and configure a Channel database item, you need to be logged on to ClearSCADA with a User account that has the Configure Database feature enabled and the relevant permissions set (see Creating a User Account in the ClearSCADA Guide to Security).

The number of channels that you need to configure, along with the channel's Connection Type and setup varies, depending on the radio Series, the chosen interface, and ClearSCADA's access to the radios in the radio network (see Required Communication Setups).

You configure the Channel database item by using the Advanced Trio Diagnostics Radio Channel configuration Form (see Display a Form in the ClearSCADA Guide to Core Configuration). The Form includes a number of tabs. The tabs and the properties on those tabs are common to channels on many drivers (see Tabs on Channel Forms in the ClearSCADA Guide to Advanced Drivers).

Further Information

Configuring a Channel in the ClearSCADA Guide to Advanced Drivers. (A Trio Radio Channel is a Direct channel.)

Minimum Configuration.


Disclaimer

ClearSCADA 2017 R3