Define the Data Polling Intervals

With Trio radios other than D Series, you can configure up to 4 'normal rate' polling intervals, and up to 4 'promoted rate' polling intervals per radio. You use the polling intervals to define the frequency with which ClearSCADA polls the radio for diagnostics data. By associating different polling intervals with different points on the radio, you can configure ClearSCADA to scan for some types of diagnostic data at different rates to other diagnostics data on the same radio.

D Series radios have limited functionality compared with other supported series of Trio radios. You can only configure 1 'normal rate' and 1 'promoted rate' polling interval on a D Series radio.

To configure the required polling rates, you use the Polling Intervals section of the Radio tab:

On the configuration Form of each point that is associated with the radio, use the Retrieval Interval field to specify the polling interval (1 to 4) that ClearSCADA is to use for that particular point (see Configure the Common Point Properties). (With points on D Series radios, only Retrieval Interval 1 is valid.)

 

You can also assign a Scan Group to each point (see Configure the Common Point Properties). If required, you can use the Scan Group to provide confidence that the point's data is still up-to-date, even if the point's value has not changed for some time in the radio (however, do be aware that by using Scan Groups, this will result in additional updates to the database, so you should consider whether such additional updates are required). If used, whenever a Scan Group interval expires, ClearSCADA will attempt to scan the radio for the data of those points to which that particular Scan Group applies. To avoid unnecessary additional polling of the radio, we recommend that you configure a point's Scan Group interval so that it is a multiple of the point's Retrieval Interval.


Disclaimer

ClearSCADA 2017 R3