Edit an Extra Alarm Column

You can change the configuration of any of the extra columns on an alarm display at any time.

To change the configuration of an extra column on an alarm display:

  1. Display the Extra Alarm Columns Window.
  2. Select the name of the column that you want to change.
  3. Select the Edit button to display the Configure Alarm Column window.
  4. Use the Configure Alarm Column window to alter the configuration of the extra column as required. The Configure Alarm Column window works in the same way as described in Add an Extra Alarm Column.
  5. Select the OK button to confirm your selections and close the Extra Alarm Columns window.

Disclaimer

ClearSCADA 2017 R3