Why are Alarms Becoming Enabled or Disabled Unexpectedly?

If your database has items that have their alarms enabled or disabled unexpectedly, the most probable cause is that:

When the Independent feature is disabled on the server:

Example:

Your server settings could define a 1 hour Fixed Duration for Disable Alarms. So when you select Disable Alarms for a point, you may expect the point’s alarms to be disabled for an hour. This may not be the case, as a Logic program, Schedule or Method Call could trigger Enable Alarms within the hour period. If Independent is disabled, the Enable Alarms action is applied, irrespective of the hour period.

If Independent is enabled:

Further Information

Independent: see Define whether User Types can Disable Alarms Independently in the ClearSCADA Guide to Server Administration.


Disclaimer

ClearSCADA 2017 R3