Configuring the Aquis Server

The Aquis Server database item provides the settings needed by the Aquis Thin Client to connect to the Aquis application server's generic web services.

Your Aquis System Administrator will provide you with the correct server address to allow you to connect to an Aquis Server.

Use the fields on the Aquis tab of the Aquis Server form to define these settings.

Complete the following fields:


Disclaimer

ClearSCADA 2017 R3