Working with Aquis Thin Client Toolbars

There are three toolbars associated with the Aquis Thin Client display (see The Aquis Thin Client Display Window):

To display or hide any of the Aquis Thin Client toolbars:

  1. Display the Database Bar (see Display an Explorer Bar).

  2. Select and right-click the Aquis Server.
    A context-sensitive menu is displayed.
  3. Select the option(s) for the toolbar(s) that you want to display.
  4. Alternatively, deselect the option(s) for the toolbar(s) that you want to hide.

In the example illustrated the View Bar and Theme Bar have been deselected and are hidden. The Main view area expands to fill the display.


Disclaimer

ClearSCADA 2017 R3