Export to CFX

Associated with: CFX Exports

Use the Export to CFX pick action to export flow measurement data from ClearSCADA in Flow-Cal’s Common File Exchange (CFX) format. The pick action enables flow data that ClearSCADA has retrieved from any SCADAPack Modbus Flow Run(s) on the system to be exported to a suitable third-party application for data analysis.

The data that is exported includes the Flow Run’s configuration, current readings, and (if available for the time period specified) alarm log, event log, and hourly history data. If any of the latter data does not exist for the date range requested for the export, those particular section(s) in the resulting CFX file(s) will include a message to that effect (for example, ‘No Alarms’).

The Export to CFX pick action is only available if your User Account is allocated the Control security permission for the CFX Export. In addition, your User Account has to be allocated the Read and Browse security permissions for the Flow Run item(s) for which you want to export data in Flow-Cal’s CFX format.

NOTE: If the data is being exported to removable media, please check that the media is at the required location and is available for use. For example, if the data is to be stored on a CD-R, check that a suitable CD-R is in the CD-RW driver of the server before the flow measurement data is exported.

Select the Export to CFX pick action to display the Export to CFX window. Use the fields in the window to specify the Flow Run and period for which data is to be exported:

If the Use Default Path/Name when Exporting check box is clear on the CFX Export’s configuration Form (see Specify the Default Path and Output File Naming Convention), ClearSCADA displays an additional field in the Export to CFX window:

Select the OK button to trigger the export. ClearSCADA will export the data in the format that is specified on the CFX Export’s configuration Form. You can ascertain the progress of an export by monitoring its Status For more information, see CFX Specific Status Display Attributes.

Should an export be unsuccessful, ClearSCADA will raise an alarm. The alarm message will indicate the reason for the export failure. The alarm will clear once a successful export is performed. For more information, see CFX Specific Alarm and Event Categories.

If you are using this pick action with the Automation Interface, you need to specify the method name Export. (Refer to the Database Schema for argument naming conventions used with the Automation Interface.)

Example:

A typical CFX Export:

(If there is no Historic data, Alarms, or Events for the specified period of time, the export to CFX will be successful, but the tabs for which no data is available will display entries such as ‘No Alarms’ or ‘No Events’.)


Disclaimer

ClearSCADA 2017 R3