Specify Whether the Inputs used for the Gas Calculations are Live or Static

Use the check boxes in the Live Input Flags section of the CFX Export tab to specify which input data used in the Flow Runs’ calculations is ‘live’ (obtained from another device in real time) and which is static (obtained from offline analysis). Only select those check boxes for data that is calculated in real time, either directly or indirectly (for instance using a program running in the controller or other means, if direct real-time data retrieval is not supported.)

Information on whether each check box is selected or not is included with the data that is exported in Flow-Cal’s CFX format. (Some third-party flow calculation applications can handle a Flow Run’s historic data differently, depending whether the inputs used for the Flow Run’s calculations are live or static.)


Disclaimer

ClearSCADA 2017 R3