Edit an Existing ViewX Client - System Connection

You can use the ClearSCADA Client Applet to change the configuration of an existing ViewX client - system connection. This is useful when you need to alter the way the client - system connection works, for example, you may need to reconfigure the port settings to avoid clashes with other applications.

The settings for a ViewX client - system connection work in exactly the same way as when used during the initial configuration of the client - system connection.

To edit an existing ViewX client - server connection:

  1. Display the ClearSCADA Client Applet.
  2. Select the client - system connection that you want to edit.
  3. Select the Edit button to display the ClearSCADA Client Configuration window (see Display the Client Configuration Window).
  4. Define the System Name and Type for a ViewX Client - System Connection.
  5. Enable or Disable Client Licensing.
  6. Define Whether the System is Visible in ViewX.
  7. Define the Node Name for a Client - System Connection.
  8. Define the Node Cost for a Client - System Connection.
  9. Define the Client Compression Settings for a ViewX Client Connection.
  10. Define the Port and Poll Timeouts and Intervals for a ViewX Client Connection.
  11. Define the TCP/IP Tuning Settings for a ViewX Client - System Connection.
  12. Change the Range of Ports for the Client’s Incoming Data.
  13. Associate a ViewX Client - System Connection with a Client License.

Alternatively, you can edit the Systems.xml file manually (see Use the Systems.xml File to Set Up a ViewX Client Connection).


Disclaimer

ClearSCADA 2017 R3