Failed Third Party OLEDB Client - System Connections

If the OLEDB client - system connection cannot be established, the OLEDB client will be unable to connect to ClearSCADA.

The connection may fail to establish if:

The firewall rules for Third Party OLEDB Client - System connections are the same as those for ViewX - system connections.

Further Information

Firewall Settings for Client - System and Server Advise Connections.


Disclaimer

ClearSCADA 2017 R3