Combo Box

To enter data using a combo box, you click on the arrow to display a pop-up list of options, and select the option that you require. The highlighted value is then displayed in the field.

With some combo boxes, you can also type the value directly into the field.

Be aware that if the Dictionary feature is used on your system, some strings in combo box lists may be prefixed with @, to enable those strings to be ‘translated’, so that they are replaced by other terms, when displayed on a List, Mimic or Trend in ViewX.

For more information on using the Dictionary feature, see Introduction to the ClearSCADA Translation Dictionary in the ClearSCADA Guide to the Translation Dictionary.


Disclaimer

ClearSCADA 2017 R3