Configure the Basic Properties of a Variable

To configure the basic properties of a Variable, display its configuration Form (see Display a Form). Most Variable Forms have only two tabs—configure the required properties on these tabs. The tabs comprise:

The Constant Double Variable has an additional tab:

Further Information

Set the Value of a Variable, other than a Constant Double Variable.


Disclaimer

ClearSCADA 2017 R3