Delete a Field from a Data Set

You can delete single or multiple obsolete fields from a Data Set, while that Grid is displayed in Design mode (see Edit a Data Set).

To delete field(s) from a Data Set:

  1. Select the required field(s) in the Data Set.

  2. Either:
    • Press the Delete key.

    or:

    1. Right-click on the obsolete field(s).
      A context sensitive menu is displayed.
    2. Select the Delete option.

    or:

    • Select the CTRL + X keys.
  3. Save the configuration.

Further Information

Keyboard Shortcuts


Disclaimer

ClearSCADA 2017 R3