Display the Add Action Window or the Edit Action Window from a Schedule

You typically display the Add Action window when you Add an Action to a Schedule, or when you Edit a Scheduled Action.


You can use either window to Specify a Method (action) that ClearSCADA is to trigger automatically on a scheduled basis.

You can additionally use the Edit Action window to change the database item on which ClearSCADA is to perform the action.


Disclaimer

ClearSCADA 2017 R3