Organizing and Configuring Your Database

When first setting up or expanding an existing ClearSCADA system, you need to plan your requirements for the Database Structure and Database Security on your system. You should do this before you start any configuration within ClearSCADA. For a summary of the planning aspects that should consider, see Preparation.

Once the plan is in place, you can use various features within ClearSCADA to rapidly configure your database (see Add an Item to the Database).


Disclaimer

ClearSCADA 2017 R3