Parameters

Parameters are stored as configuration in the ClearSCADA database. Parameters are intended to store static values and can be used as an alternative to custom fields.

Create and configure a Parameter on your system if you require:

If using String Parameters, consider using a Parameter Table, rather than a series of String Parameters, if a set of up to four String Parameters is required.

Further Information

Add a Parameter

Configure a Parameter

Example Configuration

Importing and Exporting Database Items


Disclaimer

ClearSCADA 2017 R3