Specify a Postal Address

Use the Address tab on an Address Parameter’s Form to specify the postal address that the Parameter is to store.

The address can comprise up to four lines, including the Region (for instance, a county or state) and the Postal Code.

The Address 1, Address 2, and Region fields can each comprise up to 64 alphanumeric characters, including spaces.

The Postal Code can comprise up to 20 alphanumeric characters, including spaces.


Disclaimer

ClearSCADA 2017 R3