Specify the Period Over which Historic Data is Calculated

Use the Window Start and Window End fields to specify the period for which ClearSCADA is to calculate historic data.

If the expression includes a comparison between the data values of two or more points, ensure that the calculation period is large enough to include the sample data from all of the source points. (In effect, the Historic Calculation re-samples all of the historic data that is used in its expression, in order to produce historic data for the Target point.)

For a further example of how to use the above fields, see Example Configuration.


Disclaimer

ClearSCADA 2017 R3