Types of Schedule Display

You can configure five different types of Schedule, as appropriate to your system requirements. The Schedule Display that operators can view to check for scheduled events, or that engineers can use to configure trigger times and scheduled actions, varies, depending on the Schedule type.

The divisions on each Schedule Display (other than that for a Simple Schedule) adjust in relation to the size of the window—to display the greatest number of divisions, maximize your ViewX window and the size of the Schedule Display.


Disclaimer

ClearSCADA 2017 R3