Configure the Error Handling Options for a Calculation Point

Use the fields in the Error Handling section of the Calculation tab to specify what should happen if ClearSCADA detects an anomalous condition when it evaluates the calculation expression. Example anomalous conditions could be: a divide by zero condition or a type mismatch condition.


Disclaimer

ClearSCADA 2017 R3