Configuring a Point

For each measuring instrument or control device on your system, you need to create and configure a corresponding Point of the appropriate type within the ClearSCADA database (see Types of Point used in ClearSCADA). The point configuration allows the corresponding plant to be measured or controlled from the ClearSCADA server. It also allows you to define how that point data is displayed and used within ClearSCADA. For instance, whether the raw value is scaled for use within ClearSCADA, and whether ClearSCADA logs an event or raises an alarm if the point goes into a particular state.

To create and configure a point in the database, you need to be logged on via a User Account that has the Configure Database feature enabled, and has the relevant permissions (see Creating a User Account, in the ClearSCADA Guide to Security). You also need to have carried out any necessary Preparation, to enable you to configure the point(s) successfully in the database.

You configure each point by entering data into fields on a Point Form. The fields on the Form vary, depending on the type of point, and the driver with which it is associated.

Within ClearSCADA:

Regardless of the type of point that you want to configure, you use the same basic procedure for creating and configuring the point (see Create and Configure a Point).

Further Information

Types of Point used in ClearSCADA.

Group Templates and Group Instances in the ClearSCADA Guide to Core Configuration.

Abstract Item in the ClearSCADA Guide to Core Configuration.


Disclaimer

ClearSCADA 2017 R3