Edit and Display Options are not Available for any Reports

If a report can be generated and exported as normal, but the Edit and Display options are not available from the report’s context sensitive menu, check that the relevant Crystal Reports ViewX Client component is installed on the clients on which reports are to be edited and displayed.

For more information, see Installation on ViewX Clients on Which You Want to Edit Reports, and see Installation on Clients on Which You Only Want to Display or Print or Export Reports.

Also see Display Options are not Available for Reports on Original WebX Clients.


Disclaimer

ClearSCADA 2017 R3