Configure Common Properties on the DDE Tab

Use the fields at the top of the DDE tab to configure the common properties for each point. Some of the fields are common to points on many simple drivers (see Configure Common Point Properties in the ClearSCADA Guide to Simple Drivers). Fields that are specific to points on the DDE driver are explained below.


Disclaimer

ClearSCADA 2017 R3