Define the Historic Data Storage Properties

Use the fields within the Historic Data Filter section of the DDE tab to specify the type of data that ClearSCADA is to store historically for an analog point.

Use the Historic Data Filter section in conjunction with the Historic tab, which defines whether the server stores values historically for the point, and whether any unnecessary data is filtered out to reduce storage requirements (see Defining Historic Details for a Point in the ClearSCADA Guide to Core Point Configuration).

The ClearSCADA server retrieves and processes the current data values from the DDE server(s) that it monitors. Use the check box within the Historic Data Filter section to specify the type of retrieved data that ClearSCADA is to store historically for a particular analog point:


Disclaimer

ClearSCADA 2017 R3