Specify NetDDE Properties

The DDE server with which ClearSCADA communicates can reside on the same or another node to the server(s) on which the ClearSCADA database resides.

Use the fields within the NetDDE section of the DDE tab to specify whether the DDE server is on the same node as the ClearSCADA database, or is a NetDDE server that is to be accessed remotely via a network.

Where ClearSCADA is to access a remote NetDDE server, you need to specify the user name, password, and domain of a user that has a valid logon to both machines (the ClearSCADA server and the DDE server).


Disclaimer

ClearSCADA 2017 R3