Downloaded Security File

Associated with: DNP3 SCADAPack E Outstations and DNP3 SCADAPack Remote E Outstations that use DNP3 secure authentication.

This status attribute indicates:

This status attribute is only displayed if the Download Security Configuration pick action has been used to successfully download a security configuration file to the outstation. (Each file comprises an .rtk file that has been imported into ClearSCADA using a DNP3 SCADAPack Security Configuration database item.)

Use this status attribute in conjunction with the Downloaded Security Description attribute to ascertain information about the .rtk file that was last downloaded to the outstation.

For more information, see Import and Download SCADAPack Security Configuration Files.


Disclaimer

ClearSCADA 2017 R3