IO Module Failed

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve SCADAPack ES Remote I/O information.

This status attribute indicates whether this particular remote I/O module has failed. The module’s status is assessed by the outstation with which the I/O module is associated. The outstation then reports the status to ClearSCADA.

Possible states: True, or False.


Disclaimer

ClearSCADA 2017 R3