Specify the Outstation from which ClearSCADA is to Retrieve Status Information

Use the Outstation field on the Parent tab to specify the DNP3 SCADAPack E outstation from which ClearSCADA is to retrieve status information:

Use the field’s browse button to display a Reference browse window. Select the required outstation entry from the window.


Disclaimer

ClearSCADA 2017 R3