Use the fields on the SCADAPack tab of each DNP3 SCADAPack E Outstation Form to:
- Configure Automatic Configuration Download
- Specify Whether to Ignore an FC Not Implemented Error
- Specify Whether a Download Configuration Request Requires Confirmation
- Specify the IEC 61131-3 Version Running in the Outstation
- Specify the Outstation Identification Strings
- Configure the Unsolicited Message Properties that are Specific to a Particular DNP3 Master
- Configure Unsolicited Message Generation
- Configure Event Configuration
- Configure the DNP Route Table and Modem Authentication Properties
- Configure the Data Link Layer Setup Properties
- Configure Application Layer Properties
- Configure Network Access Parameters
- Configure the Modem Parameters
- Configure the Trend Retrieval Properties
- Configure Data Concentrator Properties
- Configure Modbus Properties
- Configure SCADAPack ES Remote I/O Properties
- Configure the Profiler and ISaGRAF Time Zone Properties
- Specify the Profile Type
- Configure Low Voltage Alarm Level
- Configure Scratchpad String Points
- Configure the Firmware Image Properties
- Configure the Security Configuration Properties.