Successful Dial Outs

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve Port Status information.

This status attribute indicates the number of times that the outstation has dialled out successfully via this port.

Also see Failed Dial Outs.


Disclaimer

ClearSCADA 2017 R3