Display Information about a Creatable Class

To display information about a creatable class, you need to access the Creatable Classes page. This is the first page that is displayed when you Access the Database Schema. It lists the classes of item that you can create in the database.

The Creatable Classes page has a hyperlink for each class of database item. If you select a hyperlink, the information for the relevant class of item is displayed (see Class Information). The information is shown in a table, and is categorized.

There is also a link to List All Classes. When you select this link, a list of every class, not just the creatable classes is shown (see Display Information about All Classes).

Further Information

Creatable Classes: see Classes.


Disclaimer

ClearSCADA 2017 R3