Protocol Alarm

Associated with: Outstations, including Slave outstations that support reporting of protocol problems

This status attribute is only displayed for outstations that can report whether there is a problem with the protocol that is being used to communicate with the outstation.

Possible states: Displays one of the Standard Alarm States.

An entry is logged in the Event Journal if a protocol alarm is raised. The message includes further information about the alarm.


Disclaimer

ClearSCADA 2017 R3