Switching

Associated with: Shared and Switched outstation sets; Shared outstations that are ‘Independent’

This status attribute indicates whether switching of outstations from one channel to another is Enabled or Disabled.

With Switched outstation sets, you can specify the number of outstations that ClearSCADA needs to detect as having failed on a channel, before the set switches lines (see Defining Channel Settings for a Switched Set in the ClearSCADA Guide to Advanced Drivers).

Further Information

Disable Switching.

Enable Switching.

Switch Line.


Disclaimer

ClearSCADA 2017 R3