Tune Alarm Limits

Associated with: Analog and Counter-type points that support this feature

This pick action is only available on a point on which:

Use the Tune Alarm Limits action to temporarily alter a point’s alarm limits during exceptional circumstances. For instance, in bad weather conditions when a flood situation is known to exist, you might want to tune a point’s limits to stop unnecessary alarms from being raised.

Select the Tune Alarm Limits pick action to display the Tune Alarm Limits window.

The window indicates the limits that are currently in force. The number of limits varies, depending on the type of point. For analog points, ClearSCADA displays the point’s full range of values in parentheses on the right-hand side of the window. The point's full range is defined in the Alarm Limits section of the point's form. The labels used on point forms for the range fields vary between drivers. For example, Zero Scale to Full Scale or Underrange to Overrange.

The Alarm Limits can appear as a grouping on the point form or as a separate tab, depending on the driver. For more information about a driver’s Alarm Limits, see the documentation for the relevant driver.

Select the check boxes of those limit(s) that you want to tune and then specify the required temporary limits in the adjacent fields. Specify values that are within the range that is configured for the point.

Tuning does not change the values of the alarm limits on the point’s configuration Form.

When tuning is in force:

Also see Tune M/S Alarm Limits.

To remove any tuning, display the Tune Alarm Limits window and clear all of the check boxes. An entry will be logged in the Event Journal, stating that the Alarm Limits have been returned to their configured defaults.

NOTE: If using this pick action with the Automation Interface, you need to specify the method name TuneLimits.


Disclaimer

ClearSCADA 2017 R3