Comparison Operators

The following table shows the comparison operators you can use in your expressions. In the descriptions, expression 1 refers to the expression to the left of the operator and expression 2 refers the expression to the right of the operator.

Operator

Symbol

Meaning

Equality

=

Compares one expression against another to see if they are equal.

It is True if expression 1 is equal to expression 2, otherwise it is False.

Inequality

<>

Compares one expression against another to see if they are not equal.

It is True if expression 1 is not equal to expression 2, otherwise it is False.

Less than

<

Compares one expression against another to see if the first expression is less than the second expression.

It is True if expression 1 is less than expression 2, otherwise it is False.

Greater than

>

Compares one expression against another to see if the first expression is greater than the second expression.

It is True if expression 1 is greater than expression 2, otherwise it is False.

Less than or equal to

<=

Compares one expression against another to see if the first expression is less than or equal to the second expression.

It is True if expression 1 is less than or equal to expression 2, otherwise it is False.

Greater than or equal to

>=

Compares one expression against another to see if the first expression is greater than or equal to the second expression.

It is True if expression 1 is greater than or equal to expression 2, otherwise it is False.


Disclaimer

ClearSCADA 2017 R3