FloBoss Digital Point
You can use a FloBoss Digital Point object to read and write (control) any value from a FloBoss that is specified by a Type, Location, and Parameter (TLP) that holds a numeric value. For a list of the numeric formats that are supported, see the table in the topic about the FloBoss Numeric Point.
The numeric value that is read from the FloBoss is converted to a digital value in ClearSCADA, allowing for easy presentation of data in a digital format. Either the entire value that is read from the FloBoss can be converted to a digital value, or up to three bits of data can be extracted from the numeric value.
For more information about the FloBoss Digital Point, see the following topics: