Why are the points that read gas composition not updated when the ChangeGasComp method is executed?

When the ChangeGasComp method is called on the FloBoss Scanner, the driver task gets a read only collection of points that are attached to the scanner. As the references are read only, their values cannot be updated during the method call.

You do not actually need to have points that read the gas composition in order to call the ChangeGasComp method.


Disclaimer

ClearSCADA 2017 R3