Hilscher Specific Status Display Attributes

Every item in the ClearSCADA database has its own Status display (also referred to as a View window or View dialog). You view an item's Status display by selecting that item's View Status pick action or menu option. The Status display provides information about the status of the selected item, presenting the information in the form of 'status attributes'. For further information about working with Status displays, see Status Displays.

Example:

The Status display for a Hilscher IO Image Analog Point provides information about the present state of the individual point.

The database items that are associated with this simple driver support a combination of:

NOTE: The Status attributes Primary Assign, Primary Eavesdrop Tx Assign, Secondary Assign, and Secondary Eavesdrop Tx Assign are not used by the Hilscher driver and can be ignored.


Disclaimer

ClearSCADA 2017 R3