Specify the Default Control Action

You can define a Default Action for IEC 60870-5 Digital Output Points. The action you choose will be performed whenever ClearSCADA sends a control request for the relevant point on the outstation. To find out which default actions are supported, please refer to the outstation’s interoperability Profile document.

To define the Default Action for an IEC 60870-5 digital output point, you need to use the Default Action setting on the Control tab of the IEC 60870-5 Digital Output Point Form:

Use the field’s combo box to select the relevant option:


Disclaimer

ClearSCADA 2017 R3