System Analysis

The analysis of IEC 60870-5 KEMA items is identical to standard IEC 60870-5 items.

Refer to IEC 60870-5 Driver System Analysis. in ClearSCADA Guide to IEC 60870-5 Drivers.


Disclaimer

ClearSCADA 2017 R3