Configuring a Kingfisher Outstation Set

The Kingfisher driver supports these types of Kingfisher outstation set:

Specify the features of each set using the fields on the appropriate Kingfisher Outstation Set Form.

Each Form has several tabs. This section explains the driver-specific fields on the Kingfisher tab of each Form. For information on the fields on other tabs, see Tabs on Outstation Set Forms.

Use the Kingfisher tab to:

For information on the minimal amount of configuration that you can undertake to produce a functional Kingfisher Outstation Set, see Minimum Configuration.


Disclaimer

ClearSCADA 2017 R3