Introduction to the Kingfisher Driver

This driver is an advanced driver. It provides additional functionality to enable ClearSCADA to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring Kingfisher items and features in the ClearSCADA database.

The guide also contains information for:

Document Scope

This guide explains the configuration, features and database items that are specific to ClearSCADA’s Kingfisher driver. The Kingfisher driver enables ClearSCADA to communicate with Kingfisher RTUs using the Kingfisher protocol.

Kingfisher Remote Terminal Units (RTUs) or outstations are used to monitor data and provide operator interaction. They are used on systems in a variety of industries, including water distribution, waste water, oil and gas.

The Kingfisher Driver allows the ClearSCADA system to communicate with Kingfisher outstations, either directly or remotely. It provides the server with extra functionality for interacting with the instruments and devices that are connected to each outstation.

You can configure ClearSCADA to communicate directly with multiple Kingfisher outstations. Alternatively, you can set up ClearSCADA to communicate with multiple Kingfisher outstations via a Kingfisher master outstation (a Master/Remote setup).

 

In a Master/Remote setup:

The Kingfisher driver in ClearSCADA allows you to configure Master/Remote scenarios that communicate using the Kingfisher protocol (see Typical Master/Remote Scenarios).

The Kingfisher protocol allows Kingfisher remote outstations to report event data independently of polling cycles. When communicating in this way, the remote outstation reports event data by transmitting unsolicited messages (also referred to as unsolicited responses). A user can program a remote outstation to send event data in these messages, at a specific time, or in response to a specific trigger.

 

To communicate with Kingfisher outstations via a Kingfisher Master outstation, ClearSCADA uses:

 

The Kingfisher Driver documentation explains how to configure Kingfisher-specific features and items within the ClearSCADA database (see Configuring Kingfisher Devices in ClearSCADA).

It also explains:


Disclaimer

ClearSCADA 2017 R3