Significant Change Properties

Use the fields within the Significant Change section of the tab to define the amount by which a counter point’s current value has to change before it is reported to the ClearSCADA server.

Use the Significant Change feature to help prevent excessive database updates. It allows you to define whether a counter point’s value change is stored in the database or is deemed as insignificant and is discarded. If ClearSCADA discards a value, the counter point’s previous recorded value is retained in the ClearSCADA database.

The Significant Change feature applies only to current data (it does not apply to logged data). The driver applies the significant change Deadband whenever it receives a new current value for the point. The driver uses the Deadband to determine whether or not to pass the point update to the database server.

Configure the required settings using these fields within the Significant Change section of the tab:


Disclaimer

ClearSCADA 2017 R3