Use Persistence to Stop Fleeting Changes in Value from Changing the Point State

Use the fields within the Persistence section of the Digital Point tab to stop fleeting changes in value from causing a change in point state. With the Persistence feature, a change in value will only cause a change in point state if that point remains in the new state for a specified time.

For information on defining the Persistence times, see Use Persistence to Stop Fleeting Changes in Value from Changing a Point State.


Disclaimer

ClearSCADA 2017 R3