User-Specific Events List Preferences

This section summarizes those Events List options that a system administrator can configure on a per-user basis. The options apply to users that log onto the system using a User Account.

The options for each individual User Account, if they are to differ from the defaults, should be specified when the User Account is added to the system.

For a user that logs onto the system using an individual User Account, use that user’s User Form to:

For information on configuring any of the above, see Creating a User Account in the ClearSCADA Guide to Security.


Disclaimer

ClearSCADA 2017 R3